Objekt: PROFINET IO Controller
The PROFINET IO controller, like the slaves, is identified by the station name. For AC500 communication modules, you can also configure the IP settings here. Otherwise the settings apply from the superordinate Ethernet node.
|
“Station name” |
The station name of the device. It is used for unique identification of the device in the network. |
|
“IP address” |
Note: Available for AC500 communication module only. If you insert the controller below an Ethernet adapter, then you need to define the IP parameters in the dialog of the Ethernet adapter. |
|
“Subnet mask” |
The subnet mask used by the device. |
|
“Default gateway” |
The default gateway used by the device. |
|
“First IP address” |
Range of IP addresses which CODESYS uses by default when inserting PROFINET Devices into the device tree. If you use the “Auto-IP” function in the scan dialog, then IP addresses are also used from this range. The next free IP address is selected here. |
|
“Last IP address” |
|
|
“Subnet mask” |
|
|
“Default gateway” |
|
“Application stop –> Substitute values” |
When the user stops the application, the provider state for the output data sent by the controller is set to "BAD". Then the slaves set the inputs and outputs to predefined substitute values. For more information, see "CODESYS Default values – PROFINET Substitute values" at the end of this chapter. |
|
“Add to I/O mapping” |
|
|
“Substitute Input-Data” |
If a device does not provide valid input data, then the values (%I) in the local controller application are optionally reset or retain their last valid value |
|
“Peer station/port” |
Neighboring device with port that is connected to this port. You can accept this setting on the “ PROFINET Controller Topology” tab. |
|
“Check cable length” |
Length of the network cable (in meters)
When the cable length is specified, it is checked when the controller is powered up. An incorrect cable length causes an error message. |
|
“Transmission rate” |
Transmission rate of the connection |
|
“Disable fixed rate / autonegotiation” |
|
|
“DCP Boundary” |
|
|
“PeerToPeer Boundary” |
|
|
“Disable port” |
|
|
“Enable” |
Note: Available for AC500 communication module only.
The defaults for the watchdog originate from the device description. |
-
Default values – PROFINET Substitute values
: The incoming status information is added to the
: The transmission rate is fixed, automatic detection (autonegotiation) is disabled.
: If the