The parameter “PLC behaviour after voltage dip” allows to set the behavior of the CPU in case of short voltage dips.
If the default setting “Halt” is used, the CPU is changed to STOP mode if a short voltage dip >10 ms occurs. A new powercycle is required.
If the setting “Reboot” is used, CPU will reboot after power supply has recovered to nominal value.