'Insert' 'Jump' in FBDPermalink

fupsymb_einf_sprung (AC500-S PT)

Shortcut: <Ctrl>+<L>

This command inserts a jump. Depending on the selected position, insertion takes place directly in front of the selected input (Cursor Position 2), directly after the selected output (Cursor Position 4) or at the end of the network (Cursor Position 6).

⮫ “Cursor positions in FBD”

For an inserted jump, a selection can be made accompanying the entered text "???", and the jump can be replaced by the label to which it is to be assigned.