Command file SDCARD.INIPermalink

Only advanced users should apply the instructions in this chapter.

[FirmwareUpdate]

0 = No update

CPUFW=x

x= 0, 11, 12, 13

11 = Update system firmware using the file specified in module section [CPU] and the component path key “CPUFW”.

12 = Update with a different version; performed only if the specified version of the file specified by the component path key “CPUFW” in the module section [CPU] differs from the current version of the CPU.

13 = Update with newer version, performed only if the version of the file specified by the component path key “CPUFW” in module’s section [CPU] is newer than the current version of the CPU.

BootFW=x

x= 0, 11, 12, 13

See description of CPUFW. The component path key for the boot firmware in the module section [CPU] is “BootFW”.

UpdateFW=x

x= 0, 11, 12, 13

See description of CPUFW. The component path key for the update firmware in the module section [CPU] is “UpdateFW”.

DisplayFW=x

x= 0, 11, 12, 13

See description CPUFW. The component path key for the display firmware in the module section [CPU] is “DisplayFW”.

UpdateHook=x

x= 0, 11

11 = Execute UpdateHook using the file specified in the module section [CPU] and the component path key “UpdateHook”.

ImportLicense=x

x= 0, 12

12 = Import the license using the file specified in the module section [CPU] and the component path key “ImportLicense”. The license file is a Wbb or WibuCmRaU file. The update process imports this file into the PLC.

Note: Do not use parameter 11 for license import.

ExportLicense=x

x= 0, 12

12 = Export the license to the file specified in the module section [CPU] and the component path key “ExportLicense”. The exported license file is a WibuCmRaC file.

Note: Do not use parameter 11 for license export.

Coupler0=x

x= 0, 11, 12, 13

0 = No update.

11 = Update firmware using the file specified in the module section [Coupler0] and the component path key “Boot” and/or “Firmware”.

12 = Update with different version; the update is only performed if the version of the file specified by the component path key “Boot” and/or “Firmware” in the module section [Coupler0] differs from the current version of the communication module.

13 = Update with newer version; the update is only performed if the version of the file specified by the component key “Boot” and/or “Firmware” in the module section [Coupler0] is newer than the current version of the communication module.

Coupler1=x

x= 0, 11, 12, 13

Update module slot 1; see description Coupler0, module section is [Coupler1]*.

Coupler2=x

x= 0, 11, 12, 13

Update module slot 2; see description Coupler0, module section is [Coupler2]*.

Coupler3=x

x= 0, 11, 12, 13

Update module slot 3; see description Coupler0, module section is [Coupler3]*.

Coupler4=x

x= 0, 11, 12, 13

Update module slot 4; see description Coupler0, module section is [Coupler4]*.

Coupler5=x

x= 0, 11, 12, 13

Update module slot 5; see description Coupler0, module section is [Coupler5]*.

Coupler6=x

x= 0, 11, 12, 13

Update module slot 6; see description Coupler0, module section is [Coupler6]*.

[UserProg]

0 = No update.

UserProgram=x

x= 0, 11

11 = Update user program always with the file specified in the module section [CPU] and component path key “UserProgram”.