Symbol: 
Function: The command opens the “Security Screen” view.
Call:
-
“View” menu
-
icon or
in the status barThe icon is displayed in blue when a valid certificate is specified for the digital signature. When only one client certificate is specified for the encrypted communication, the icon remains gray, resulting in the client certificate providing no increased security for the user.
The following security features of CODESYS are configured and displayed in the view:
-
Personal user certificate
-
Encrypted communication
-
Encryption and signatures of IEC projects
-
Encryption and signature of download, online change, and boot application
-
Security level




NOTICE

When the “Security Screen” is opened and closed, the current settings are applied in the user options, even when no active changes have been made.
If the CODESYS Security Agent add-on product is installed, then the “Security Screen” view provides an additional “Devices” tab. This allows for the configuration of certificates for the encrypted communication with controllers.
Tab 'User'
On this tab, certificates are configured that are required for the encrypted communication and the digital signature of the user. Only certificates with private keys can be specified here. The user profile is saved as an XML file in the user options.
|
“User Profile and Certificate Selection” |
By default, the login name for Windows is specified as the user profile. |
|
List box with existing user profiles |
|
|
“Digital Signature” |
One certificate can be selected. The certificate has to have a private key.
One certificate can be selected. The certificate has to have a private key. |
|
“Project File Decryption” |
One certificate can be selected. The certificate has to have a private key.
|
See also
|
“Activate the Use of Certificates for Enhanced Security” |
|
|
“Enforce encrypted communication” |
|
|
“Enforce encryption of project files” |
To open this project, the certificate to be encrypted has to be specified in “Project file decryption” with a private key. |
|
“Enforce signing of project files” |
When a project is saved, a signature file |
|
“Enforce encryption of downloads, online changes and boot applications” |
This certificate is defined directly either in the properties dialog of the application on the “Encryption” tab, or in the security screen, on the “Project” tab, in the “Encryption of Boot Application, Download and Online Change” group. Controller certificates are located in the local Windows Certificate Store in the “PLC Certificates” directory. If the certificates of your controller are not available in the directory, then they first have to be loaded from the controller and installed to the directory. For instructions, see the "“Controller Certificates”" chapter. |
|
“Enforce signing of downloads, online changes and boot applications” |
Requirement: The “Encryption of boot application, download and online change” option is selected. |
|
“Enforce signing of compiled libraries” |
Requirements
“Enforce timestamping of signed compiled libraries”: |
Tab 'Project'
All project-specific settings are configured on this tab. These elements are active only when a primary project is loaded.
|
“Project file encryption” |
|
|
“Technology” |
When you select the “Encryption” project setting and then “Certificates” in the dialog, you can choose a corresponding certificate by clicking |
|
“Certificates of Users Sharing this Project” |
Area for listing the certificates that encrypt the project file. |
|
“Encryption of Boot Application, Download and Online Change” |
|
|
List of the applications of the controller |
Double-clicking an application in the list opens the “Properties Encryption” dialog. Depending on the settings of the “Security Level” on the “User” tab of the “Security Screen”, the following fields are available in the open properties dialog:
In the “Properties Encryption” dialog, click the Controller certificates are located in the local Windows Certificate Store in the “PLC Certificates” directory. If the certificates of your controller are not available in the directory, then they first have to be loaded from the controller and installed to the directory. For instructions, see the "Protecting and Saving a Project" - " Encryption with Certificates" chapter. |
Tab 'Devices'
This tab is available only after you have installed the CODESYS Security Agent add-on. For a description of this tab, see the help for the CODESYS Security Agent.
: Opens the
: Deletes the selected user profile. This user profile is no longer displayed in the
list box.
: Opens the
: When the user communicates with the controller, the server certificate of the controller
is used for establishing an encrypted connection. Then the entire communication is
encrypted.
: Opens the