Function: The dialog contains the properties of the application for encryption. If the CODESYS Security Agent is installed, then you can start a wizard for the encryption of downloads, online changes, and boot applications.
Call:
-
Menu bar: “View Properties”
-
Context menu of an application object
|
If the “Enforce encryption of downloads, online changes and boot applications” option is selected in the “Security Screen” view in the “Security level” group, then the encryption technology is set to “Encryption with certificates” and cannot be changed in this dialog. |
|
|
“No Encryption” |
|
|
“Simple Encryption” |
You can download the boot application to the controller only when the defined dongle (license key) is connected to the computer. The dongle is provided by ABB AG or by the respective hardware manufacturer. The firmcode is displayed. Type in the delivered product code. |
|
“Encryption with license management” |
You can download the boot application to the controller only after you have specified the product code and firmcode, and the respective dongle is connected to both the development computer and the controller. You receive the codes from the vendor that manages the licenses. |
|
“Encryption with certificates” |
You can download the boot application to the controller only when a valid certificate exists for it. The “Certificates” group is enabled. See the description below. The option is already selected if the “Enforce encryption of downloads, online changes and boot applications” option is selected on the “User” tab of the “Security Screen” view. You can also select the “Digitally sign application code” option. |
|
Note: If the “Enforce encryption of downloads, online changes and boot applications” option is selected in the “Security Screen” view in the “Security Level” group, then the encryption technology is set to “Encryption with certificates” and cannot be changed in the “Properties” dialog. |
|
|
|
The “Certificate Selection” dialog opens. Here you can select previously installed certificates of devices for which the encryption of download, online change, and boot application is enabled. The list can contain several entries if several devices are authorized to run this application. |
|
“Digitally sign application code” |
The application is signed with a digital signature. The certificate for the digital signature is specified in the “Security Screen” view on the “User” tab. |
|
Area for the display of the selected certificates with corresponding information |
Information per certificate:
|
|
“Encryption Wizard” |
This button is available only if the CODESYS Security Agent is installed. It starts the wizard with the same name. See the help for CODESYS Security Agent in this case. |
See also
-
Help about CODESYS Security Agent
: