Function: This command loads the project source code (as project archive) from the controller.
Call: Main menu “File”.
Requirement: The network path for the controller must be configured.
After you execute the command, an overview opens with all devices in the network. Select a controller from this overview. The dialog box “Extract Project Archive” then opens with export settings.
See also
Dialog Box 'Extract Project Archive'
This dialog box shows the contents of the project archive. You can exclude complete
categories or single objects from categories by clearing the check boxes (
) from the extraction.
|
“Extract into the same folder where the archive is located” |
The archive is extracted to the same directory. |
|
“Extract into the following folder” |
The contents of the archive are extracted to the given path. |
|
“Advanced” |
Opens the “Advanced” dialog box for you to define where special and additional files from the archive are extracted. |
|
“Items” |
Shows the contents of the archive structured in object categories.
|
|
“Comment” |
Comment that was entered when creating the project archive |
|
“Extract” |
If an extracted file has the same name as an existing file in the target directory,
then a dialog box opens, prompting whether the local file should be replaced. The
decision can be applied automatically to any additional conflicting names. In this
case, you have to select the |
: The object is not extracted.