You can customize the menu commands of the CODESYS user interface. In a configuration dialog, you can add or remove menus.
Removing menus and commands
- 
                           
Choose the command “Tools Customize”.
The “Customize” dialog box opens. The “Menu” tab is visible.
 - 
                           
Select a menu in the menu tree or a command in a menu.
 - 
                           
Click “Delete”.
The menu or command is deleted from the menu tree.
 - 
                           
Click “OK”.
The dialog box closes and the menu is customized.
 
Adding menus
- 
                           
Choose the command “Tools Customize”.
The “Customize” dialog box opens. The “Menu” tab is visible.
 - 
                           
Scroll to the end of the menu tree.
 - 
                           
Select the blank symbol (
). - 
                           
Click “Add Popup Menu”.
The “Add Popup Menu” dialog box opens.
 - 
                           
Type a name for the new menu in the “Default text” field.
If localization is unnecessary, then skip to step 9.
 - 
                           
Click “Add Language”.
A drop-down list opens with available languages.
 - 
                           
Choose the required language.
The language is added to the list of languages.
 - 
                           
Click into the “Text” field and type the language-specific text.
 - 
                           
Click “OK”.
The new menu is added at the bottom of the menu tree.
 - 
                           
Change the menu order by clicking “Move up” and “Move down”. Click “OK” to close the “Customize” dialog box.
The new menu is displayed only when it contains a command.
 
Adding commands
- 
                           
Choose the command “Tools Customize”.
The “Customize” dialog box opens. The “Menu” tab is visible.
 - 
                           
Expand the branch of the menu where the new command should be added.
 - 
                           
Select the blank symbol (
). - 
                           
Click “Add Command”.
The “Add Command” opens dialog box.
The dialog box lists all commands grouped by category.
 - 
                           
Select the command to be added. Click “OK”.
The new command is added to the menu tree.
 - 
                           
Change the menu order by clicking “Move up” and “Move down”. Click “Add separator” to add a border between commands. Click
OKto close the “Customize” dialog box.The new command is now available in the menu.