Function: With this dialog, you define the structure and contents of the user interface.
Call: Main menu “Tools Customize” (“Menu”).
When you click “OK” to close the dialog, the changes are visible in the menu bar of the CODESYS user interface.
| 
                                  Display of currently defined menus, submenus, and included commands. In CODESYS, a menu or submenu caption is identified by the caption symbol (  | 
                           |
| 
                                  “Add Command”  | 
                              
                                  Enabled when a command is selected. Adds a command above the selected command. Opens the “Add Command” dialog. Use the “Add Command” dialog for selecting one or more commands. Left part: List of categories. Right part: List of commands in the selected category.  | 
                           
| 
                                  “Add Separator”  | 
                              
                                  Adds a separator above the selected command.  | 
                           
| 
                                  “Add Popup Menu”  | 
                              
                                  Adds a popup menu above the selected menu, submenu, or command. Opens the “Add Popup Menu” dialog.  | 
                           
| 
                                  “Edit Popup Menu”  | 
                              
                                  Opens the “Edit Popup Menu” dialog.  | 
                           
| 
                                  “Reset”  | 
                              
                                  Resets the default settings of the entire menu.  | 
                           
| 
                                  “Load”  | 
                              
                                  Loads the settings from a stored file (<file name>.opt.menu).  | 
                           
| 
                                  In CODESYS, a new menu is shown in the menu bar only when the menu contains at least one command.  | 
                           |
| 
                                  “Default text”  | 
                              
                                  Select this check box when localization is available.  | 
                           
| 
                                  “Localized Texts”  | 
                              
                                  List: Languages and localized texts.  | 
                           
| 
                                  “Add Language”  | 
                              
                                  Opens a drop-down list of available languages. In CODESYS, the selected language is displayed in the area “Localized Texts”. Use the “Text” column for typing the localized texts.  | 
                           
). The layout from top to bottom corresponds to the layout displayed later in the