Function: Use this dialog for generating new toolbars or customizing existing toolbars.
Call: Main menu “Tools Customize” (“Toolbars”).
When you click “OK” to close the dialog, the changes are visible in the menu bar of the CODESYS user interface.
| 
                                  Display of currently defined toolbars. In CODESYS, the associated commands are listed below each toolbar in the order they will appear in the toolbar. Double-clicking a toolbar in the list switches to editing mode.  | 
                           |
| 
                                  “Add Toolbar”  | 
                              
                                  Enabled when a toolbar is selected. In CODESYS, this adds a toolbar above the selected toolbar and places the cursor in the name field of the new toolbar.  | 
                           
| 
                                  “Add Command”  | 
                              
                                  Enabled when you select a command or blank command entry below a toolbar. Adds a command above the selected command. Opens the “Add Command” dialog. Use the “Add Command” dialog to select one or more commands. Left part: List of categories. Right part: List of commands in the selected category.  | 
                           
| 
                                  “Add Separator”  | 
                              
                                  Adds a separator above the selected command.  | 
                           
| 
                                  “Hide”  | 
                              
                                  Hide the selected toolbar from the user interface.  | 
                           
| 
                                  “Show”  | 
                              
                                  Shows the selected hidden toolbar in the CODESYS user interface.  | 
                           
| 
                                  “Reset”  | 
                              
                                  Resets the default settings of the toolbars.  | 
                           
| 
                                  “Load”  | 
                              
                                  Loads the settings from a stored file (<file name>.opt.tbar).  |