Options (Controller)
Function: This dialog provides the settings for monitoring an login for objects of type device. The availability of the options depends on the device description.
Call: Context menu of the device, or main menu “View Properties”, if the device is selected.
|
“Monitoring interval (ms)” |
Interval of the monitoring (10 ms - 1000 ms) |
|
This mode is used to prevent an accidentally login to a different controller. |
|
|
“None” |
No interaction with the user during login. Corresponds to the behavior of previous versions. |
|
“Enter ID” |
During login CODESYS asks to enter an ID. The ID is stored in the controller. Without a valid ID no login is possible. When login a second time, CODESYS does not ask again for the ID if the computer name, the user name, the device name and the device address have not changed. The information is saved in the project options. |
|
“Press key” |
During login a dialog prompts and requests the user to press a key on the controller. The timeout for this action is saved in the device description. |
|
“Wink (= blink an LED)” |
During login a led blinks on the connected controller. |
|
“Access variables in sync with IEC tasks” |
The setting only will take effect when all applications and boot applications are re-downloaded to the controller. Note: If the option is activated, then the jitter for all IEC applications may increase on this device! The consistent access can disturb the real-time capability. |
: Default setting, consistent access is not permitted
: Consistent access is permitted