You can use the symbol configuration for creating symbol descriptions for project variables. Click “Project Add Object” to add a symbol configuration object to the device tree. Then define specific presets. See dialog below: “Add Symbol Configuration”.
Double-click the “Symbol Configuration” object to open the symbol configuration editor.
Dialog 'Add Symbol Configuration'
Function: This dialog is used to define the defaults for a “Symbol Configuration” object.
Call: “Project Add Object Symbol Configuration” menu; context menu of the application object.
|
“Include comments in XML” |
Exports the symbol file with the comments assigned to the variables. |
|
“Support OPC UA features” |
Note: Availability and editability of this option depend on the device.
|
|
For detailed information and examples of layout options, see the next section "Symbol Configuration Editor". |
|
|
“Compatibility layout” |
This setting is used for the compatibility of old projects. The data layout created for the client is matched as much as possible to the layout created internally by the compiler. |
|
“Optimized layout” |
Recommended for new projects. Calculates the output layout in optimized form detached from the internal compiler layout. Does not generate any gaps for unpublished elements and strictly fulfills the requirements for memory alignment of the data types. Requires compiler version 3.5.7.0 or higher. |
Symbol configuration editor
The editor includes a table with selected variables and a menu bar for editing.
|
|
You can use this button for activating and deactivating the following categories of variables used in the configuration editor:
|
|
|
Compiles the project. Requirement for current preparation of variables in the configuration editor. |
|
|
|
|
“Download” |
If you use a device that supports its own application file for the symbol configuration,
then this button is also available in the toolbar. If you change the symbol configuration
in online mode, then you can load the new |
|
“Tools” |
“Save XSD Scheme File”: This command opens the standard dialog for saving a file in the file system. With this command, you can prepare the XSD format of the symbol file, for example for use in external programs. |
|
“Access Rights” |
You can change the access rights for a symbol by clicking the symbol in the “Access Rights” column. Icons for access rights (in ascending order)
Note: In case the controller has a user management, you can use symbol sets to define client-specific access rights to the same symbols. |
|
“Maximal” |
Maximum access rights for this symbol |
|
“Attribute” |
If the access right was assigned by attribute, then a corresponding icon is displayed here. |
|
“Type” |
Alias data types are also displayed In CODESYS V3.5 SP6 and higher. Example: |
|
“Members” |
You can add variables of a structured data type also by selecting a check box for
symbol configuration in the “Symbols” column. This causes CODESYS to export all member variable symbols. However, in the “Members” column, you can click the ellipsis button ( |
|
“List box” |
Already defined symbol sets |
|
|
Opens the “Add New Symbol Set” dialog for specifying a name for this set |
|
|
Opens the “Add Duplicate from Selected Symbol Set” dialog. A copy is created for the set selected in the list box. You can change the
default name ( |
|
|
Opens the “Rename Selected Symbol Set” dialog for specifying another name for the set selected in list box. |
|
|
Opens a dialog prompting whether or not the symbol set selected in the list box should be deleted. |
|
“Configure Symbol Rights” |
Opens the “Symbol Rights” tab of the device editor. When logged in there, you can assign different access rights for each user group (client) to the symbol set selected in the list box. |
See also
Dialog 'Comments and Attributes'
|
“Enable extended OPC UA information” |
Note: Availability and editability of this option depend on the device.
When the OPC UA setting is enabled, attributes are included in the symbol table according to the following rule:
|
|
“Include comments” |
Requirement: “Enable extended OPC UA information” is activated.
|
|
“Include attributes” |
|
|
“Also include comments and attributes for type nodes” |
Requirement: “Include comments” is activated.
|
|
“Include namespace node flags” |
|
|
“Include comments” |
In compiler versions V3.5.5.x to V3.5.8.0, this includes the setting “Prefer docu-comments”. |
|
“Include attributes” |
|
|
“Also include comments and attributes for type nodes” |
Requirement: “Include comments” is activated.
|
|
Requirement: “Include comments” is activated. |
|
|
“Include docu comments” “Include normal comments ” “Always include both types of comments” “Prefer docu comments, fallback to normal ones” “Prefer normal comments, fallback to docu comments” |
The options determines the comments that are saved in the symbol configuration. |
|
Requirement: “Include attributes” is activated. |
|
|
“Include all attributes” “Include attributes starting with” “Filter attributes with regular expression” |
Defines the attributes that are saved in the symbol configuration. |
|
“Match simple identifiers” |
Exists primarily due to the backward compatibility to older versions in order to emulate the old behavior. |
Setting: Configure synchronization with IEC tasks
For synchronously consistent access, the symbolic client waits in the runtime when processing a read or write request until a time is found when no IEC task is executed. When this gap is detected, restarting the IEC tasks is prevented until all values of the variable list have been copied. Then the IEC tasks are planned again as usual. Synchronized access can cause a delayed starting of IEC tasks, which is shown as increased jitter. As all applications in the runtime are managed by a common scheduler, this potential impairment of the real-time behavior affects all applications on the device. All applications of the device are affected, regardless of whether or not they include a symbol configuration or they have been downloaded to the controller from one or more CODESYS projects. Therefore, the runtime permits synchronized consist access only if this it allows all applications that are downloaded to the controller at the time of access.
The setting is located in the editor of the symbol configuration of the “Settings” menu. In addition, the setting is also located in the context menu of the controller when you click the “Properties” command and then select the “Options” tab in the opened dialog.
For applications without symbol configuration, the setting can only be found in the properties dialog.




NOTICE

After changing the setting, all applications downloaded to the device by means of a download or online change have to be reloaded and all boot applications updated.
In which cases is synchronized consistent access necessary?
As a rule, there is no need for consistent values for displayed values because it is mostly irrelevant from which IEC task cycle the changed values originate. It is completely irrelevant for seldom changed values. Even when writing there are almost no hard consistency demands because typically the machine must be in a kind of standby mode (for example when writing recipes) in which there is no direct access to the values written as recipes.
In contrast, consistent values are particularly necessary for database links to save
production data. For clocked machines, however, these values must be synchronous with
the production timing (one value set per produced product) and not consistent with
reference to one or more IEC tasks. With reference to the machine clocking, the consistency
must be already ensured by the IEC application. For this purpose, the values that
arise during a production cycle are typically collected in a global variable list.
At the end of the cycle, the symbolic client is notified by means of an additional
variable (BOOL or counter) that the machine cycle has ended and the values are valid. Now the client
has the chance to archive the values from the production cycle. Depending on necessity,
the successful reading can also be displayed in the opposite direction by means of
a released variable, so that the production can also be halted in case the production
data cannot be archived. Synchronized consistent access is not necessary and helpful
for this use case because the synchronization takes place at the application level.
In contrast, synchronized consistent access by symbolic clients is typically applied in the process industry with continuously running systems without production clocking when, for example when process values are written consistently and cyclically in a fixed time frame of 60s. This can take place either by synchronization on the application level similar to clocked machines (see above) or by synchronization of the synchronized consistent symbolic access. The advantage of the latter is that no logic has to be implemented in the IEC program and access is controlled entirely by the client.




CAUTION

Due to the increased jitter, the synchronized consistent monitoring is not suitable for motion or real-time critical applications. For these reasons, synchronized consistent access should be released and used only if it is absolutely necessary.
If a client uses synchronous consistent access released by this setting, then it has and effect on the client. Depending on the scheduler of the runtime, the response time can jitter more here for read/write access because the system might still have to wait for an execution gap of the IEC tasks. Read and/or write access can still fail when IEC tasks run for a long time (in the range of several 100 ms) or the CPU load is close to 100% for an extended period of time with one or more IEC tasks (in the range of several 100 ms). Therefore, the availability of the values also depends on the load of the controller by the IEC application.
Moreover, the client can minimize the effects on itself and on the runtime if it observes the following in the definition of the variable lists to be read or written:
-
Synchronized consistent access only to those variables that are absolutely and consistently required.
-
Separate variable lists for variables that have to be consistent and for variables that could be inconsistent.
-
Divide variable lists with several consistent variables into several smaller lists.
-
Select read intervals for cyclic reading of values as large as possible.
Support for the current configuration and possible corrective actions
Entries marked in red in the symbol table show variables that they are configured for export to the symbol file but are currently invalid in the application. The cause for this can be that the declaration has been removed from the block.
In version 3.5.8.0 and higher, a warning appears in the editor if variables that have configured symbols are not used in the IEC code or are not mapped in the case of I/O variables. In addition, the compiler indicates variables that are referenced from outdated library versions n the symbol configuration.




NOTICE

Object variables that are not used in the program code remain uncompiled by default and are therefore not available in the symbol configuration.
However, CODESYS provides variables from uncompiled objects in the symbol configuration when one of the following conditions is met:
-
The “Link always” POU property is selected.
-
The
{attribute 'linkalways'}pragma is used.
Example for the data layout types
Examples for the layout types
The following examples from an IEC application will show how gaps can result in the client-side memory layout caused by unpublished symbols, internal "invisible" pointers, or a "pack mode" definition in the device description. With the “Optimized layout” setting, the gaps are avoided. The symbol file contains different information about the size and offset of memory locations, depending on the selected layout setting.
Example: Large structure
// Example of a big structure, where not all members get published :
STRUCT
{attribute 'symbol':='readwrite'}
PublicNumber : INT;
{attribute 'symbol':='none'}
InternalData : ARRAY[0..100] OF BYTE;
{attribute 'symbol':='readwrite'}
SecondNumber : INT;
{attribute 'symbol':='none'}
MoreData : ARRAY[0..100] OF BYTE;
END_STRUCT
END_TYPE
Resulting entries in the symbol file; pay attention to "size" and "byteoffset":
Symbol file, large structure, compatibility layout option
<TypeUserDef name="T_LargeStructure" size="208" nativesize="208" typeclass="Userdef" pouclass="STRUCTURE" iecname="LargeStructure"> <UserDefElement iecname="PublicNumber" type="T_INT" byteoffset="0" vartype="VAR" /> <UserDefElement iecname="SecondNumber" type="T_INT" byteoffset="104" vartype="VAR" /> </TypeUserDef>
Symbol file, large structure, optimized layout option
<TypeUserDef name="T_LargeStructure" size="4" nativesize="208" typeclass="Userdef" pouclass="STRUCTURE" iecname="LargeStructure"> <UserDefElement iecname="PublicNumber" type="T_INT" byteoffset="0" vartype="VAR" /> <UserDefElement iecname="SecondNumber" type="T_INT" byteoffset="2" vartype="VAR" /> </TypeUserDef>
Example: Structure with uneven addresses
// The following mechanisms can cause memory misalignment:
// - {attribute 'relative_offset':='…'} at a member
// - {attribute 'pack_mode':='…'} at a structure declaration
// - target setting 'memory-layout\pack-mode' in the device description
{attribute 'pack_mode':='1'}
TYPE UnevenAddresses:
STRUCT
{attribute 'relative_offset':='3'}
{attribute 'symbol':='readwrite'}
PublicNumber : INT;
{attribute 'symbol':='readwrite'}
PublicValue : LREAL;
END_STRUCT
END_TYPE
Resulting entries in the symbol file; pay attention to "size" and "byteoffset":
Symbol file, structure with uneven addresses, compatibility layout option
<TypeUserDef name="T_UnevenAddresses" size="13" nativesize="13" typeclass="Userdef" pouclass="STRUCTURE" iecname="UnevenAddresses"> <UserDefElement iecname="PublicNumber" type="T_INT" byteoffset="3" vartype="VAR" /> <UserDefElement iecname="PublicValue" type="T_LREAL" byteoffset="5" vartype="VAR" /> </TypeUserDef>
Symbol file, structure with uneven addresses, optimized layout option
<TypeUserDef name="T_UnevenAddresses" size="16" nativesize="13" typeclass="Userdef" pouclass="STRUCTURE" iecname="UnevenAddresses"> <UserDefElement iecname="PublicNumber" type="T_INT" byteoffset="0" vartype="VAR" /> <UserDefElement iecname="PublicValue" type="T_LREAL" byteoffset="8" vartype="VAR" /> </TypeUserDef>
Example: Function block
// Each POU contains some implicit variables, which do not get published. Depending on the data type these might cause memory gaps of different sizes. FUNCTION_BLOCK POU IMPLEMENTS SomeInterface VAR_INPUT in : INT; END_VAR VAR_OUTPUT out : INT; END_VAR VAR END_VAR
Each POU contains some implicit variables, which do not get published. If it is a
data type such as __XWORD, then different sizes of memory gaps result in the client-side data layout, depending
on whether the system is 64-bit or 32-bit.
Resulting entries in the symbol file for 64-bit and 32-bit; pay attention to "size" and "byteoffset":
Symbol file, function block, compatibility layout option, 64-bit
<TypeUserDef name="T_POU" size="24" nativesize="24" typeclass="Userdef" pouclass="FUNCTION_BLOCK" iecname="POU"> <UserDefElement iecname="in" type="T_INT" byteoffset="16" vartype="VAR_INPUT" /> <UserDefElement iecname="out" type="T_INT" byteoffset="18" vartype="VAR_OUTPUT" /> </TypeUserDef>
Symbol file, function block, optimized layout option, 64-bit
<TypeUserDef name="T_POU" size="4" nativesize="24" typeclass="Userdef" pouclass="FUNCTION_BLOCK" iecname="POU"> <UserDefElement iecname="in" type="T_INT" byteoffset="0" vartype="VAR_INPUT" /> <UserDefElement iecname="out" type="T_INT" byteoffset="2" vartype="VAR_OUTPUT" /> </TypeUserDef>
Symbol file, function block, compatibility layout option, 32-bit
<TypeUserDef name="T_POU" size="12" nativesize="12" typeclass="Userdef" pouclass="FUNCTION_BLOCK" iecname="POU"> <UserDefElement iecname="in" type="T_INT" byteoffset="8" vartype="VAR_INPUT" /> <UserDefElement iecname="out" type="T_INT" byteoffset="10" vartype="VAR_OUTPUT" /> </TypeUserDef>
Symbol file, function block, optimized layout option, 32-bit
<TypeUserDef name="T_POU" size="4" nativesize="12" typeclass="Userdef" pouclass="FUNCTION_BLOCK" iecname="POU"> <UserDefElement iecname="in" type="T_INT" byteoffset="0" vartype="VAR_INPUT" /> <UserDefElement iecname="out" type="T_INT" byteoffset="2" vartype="VAR_OUTPUT" /> </TypeUserDef>
See also
: When downloading the symbol configuration, additional information is also downloaded
to the controller. The information below is necessary for operating the OPC UA server.
: Read only
: Write only
: Read and write
: Execute
) to select only specific structural components. Note: This selection applies to all
instances of this data type for which symbols are exported. If a member of a structured
type cannot be selected, then an asterisk (
) is displayed in the check boxes of the members to indicate that all exportable members
of that type are exported.
: Only directly exported variables have comments and attributes.