- 
                        Command 'Edit Worksheet'
 - 
                        Command 'Edit Page Size’
 - 
                        Command 'Negate'
 - 
                        Command 'EN/ENO'
 - 
                        Command 'None'
 - 
                        Command 'R (Reset)'
 - 
                        Command 'S (Set)'
 - 
                        Command 'REF= (Reference Assignment)'
 - 
                        Command 'Display Execution Order'
 - 
                        Command 'Set Start of Feedback'
 - 
                        Command 'Send to Front'
 - 
                        Command 'Send to Back'
 - 
                        Command 'Move Up'
 - 
                        Command 'Move Down'
 - 
                        Command 'Set Execution Order'
 - 
                        Command 'Order by Data Flow'
 - 
                        Command 'Order by Topology'
 - 
                        Command 'Edit Parameters'
 - 
                        Command 'Save Prepared Parameters to Project'
 - 
                        Command 'Connect Selected Pins'
 - 
                        Command 'Unlock Connection'
 - 
                        Command 'Show Next Collision'
 - 
                        Command 'Select Connected Pins'
 - 
                        Command 'Reset Pins'
 - 
                        Command 'Remove Unused Pins'
 - 
                        Command 'Add Input Pin'
 - 
                        Command 'Add Output Pin'
 - 
                        Command 'Route All Connections'
 - 
                        Command 'Remove Control Point'
 - 
                        Command 'Create Control Point'
 - 
                        Command 'Connection Mark'
 - 
                        Command 'Create group'
 - 
                        Command 'Ungroup'
 - 
                        Command 'Prepare Box for Forcing'
 - 
                        Command 'Force Function Block Input'
 - 
                        Command 'Use Attributed Member as Input'