Function: This dialog is used for configuring object-dependent properties.
Call: Menu bar: “View”; context menu of the visualization object in the “Devices” view or “ POUs” view.
Tab 'General'
|
“Name ” |
Example: |
|
“Object type ” |
visualization |
|
“Open with ” |
visualization |
Tab 'Access Control'
This tab is used for defining which user group can execute which actions on the object.
Tab 'Visualization'
This tab assigns a visualization type to a visualization.
In addition, it includes settings for window size that are used at runtime.
|
“Visualization” |
Visualization type for an ordinary or referenced visualization. Preset. |
|
“Dialog ” |
Visualization type for a visualization that opens as a dialog in its own window for an input event. The input action for this is “Open dialog”. The “Close dialog” input action closes the window. Tip: A dialog usually includes an “OK” button or “Cancel” button at the bottom edge for confirming or rejecting user input, and for closing the dialog. A simple dialog or a dialog prompt includes only a question or information and buttons for closing the dialog with either “Yes” or “No”. A dialog is part of a user interface. While a dialog is open, the rest of the user interface is usually disabled. |
|
“Numpad / keypad / dialog for input configuration” |
Visualization type for a visualization that displays a virtual numeric keypad or a virtual keyboard. It appears when the user is prompted to specify text. The input action for this is “Write variable”. Note: The interface of this visualization must also conform with the interfaces for
the standard visualizations for the numeric keypad or that keyboard that provides
the Tip: The |
|
“Dialog is opaque” |
Use this option when your drawn dialog is rectangular and opaque, containing no transparent parts. |
|
“Use automatic detected visualization size” |
|
|
“Include background image” |
|
|
“Use specified visualization size” |
|
|
“Internal” |
When editing as a library project while the project is open in CODESYS, an internal visualization is handled like all visualizations. The internal visualization appears in drop-down lists. Or in the visualization manager (“Visualizations” tab). The internal visualizations that include a linked library are not visible to you. |
See also
Tab 'Build'
This tab includes options for compiling the object.
See also
: The screen area that is covered by the dialog is not refreshed. This has a positive
effect on the character and input performance.
: The size is determined so that all visualization elements are enclosed.
: All elements are visible, but a larger background image is truncated.