When you execute a Trend, it is best to proceed with user guidance and the help of the trend wizard.
Development of a visualization with trend
-
Create an empty standard project and program at least one variable into
PLC_PRG.PLC_PRGis declared and implemented -
Add the “Visualization” object to the device tree below “Application”.
An empty visualization appears.
-
Open “Toolbox Special Control”.
-
Drag the “Trend” element to the visualization
The “Trend Recording” dialog opens with the “Recording Settings”.
-
Select the task in which the trend recording will be executed.
In general the trend recording runs in the same task as the main program, i.e. PLC_PRG.
Therefore, select
MainTask. -
Add a trend variable with “Add Variable” and assign an IEC variable from PLC_PRG to the trend variable.
-
Click “OK” to close “Trend Configuration”.
There is a newly created object of the type Trend recording under “Trend Recording Manager”. The active visualization contains a “Trend” element that is selected.
-
Click “Visualization Insert Elements for Controlling Trend Elements”.
The “Trend Wizard” dialog box opens.
-
By default, all three control elements are activated in the dialog. Click “OK” to close the dialog box.
The active visualization contains a “Trend” with control elements.
-
Set the application containing the trend objects to active.
-
Compile the application with [F11].
-
Click “Online Login”.
-
Start the application with [F5].
The target visualization appears. The visualization contains the trend diagram with the value curve of the variable. The control elements enable user inputs.
Example: Visualization of the sinusoidal trend of an IEC variable.
The following objects are implemented in the project:
-
PLC_PRG -
Visualization_Trend1 -
VisuWithTrend
PLC_PRG
PLC_PRG runs as part of the application on the controller.
PROGRAM PLC_PRG VAR iVar : INT; rSin : REAL; rVar : REAL; END_VAR iVar := iVar + 1; iVar := iVar MOD 33; rVar := rVar + 0.1; rSin := 30 * SIN(rVar);
Visualization_Trend1
Visualization_Trend1 is the object that contains the configuration of the trend recording.

VisuWithTrend
VisuWithTrend is the object that visualizes the trend.
The visualization contains four elements: one “Trend” and three control elements. The properties of the trend are defined as follows.
|
Properties |
Value |
|---|---|
|
“Trend recording” |
Visualization_Trend1 |
|
“Display cursor” |
![]() |
|
“Display tool tip” |
![]() |
|
“Show frame” |
![]() |
|
“Date Range Picker” |
|
|
“Time Picker” |
|
|
“Legend” |
|
VisuWithTrend at runtime


Trend1DateRangeSelector
Trend1TimeSelector
Trend1Legend