Configuration for example projectsPermalink

The example projects require a small PLC configuration with I/O devices, e.g., as available in the training case ‎⮫ TA5450-CASE.

Table 1: Modules for the example projects to get started with the AC500 PLC

Product name

Type

First project⮫ “Getting started with an Example project”

Second project⮫ “Adding remote PROFINET I/O expansion ”

PM5630- 2ETH

processor module

x

x

TB5620-2ETH

terminal base for processor module

x

x

DA501

analog/digital mixed input/output (I/O) module

x

x

TU516-H

terminal unit for I/O module

x

x

CM579-PNIO

PROFINET communication module

--

x

CI502-PNIO

PROFINET communication interface module

--

x

TU508-ETH

terminal unit for communication interface module

--

x

TA524

blind cap for terminal base

x

x

Connections

Fig. 3: Training case TA5450

training_case_TA5450_electrical_connection01

The training case includes the control panel CP6607. A control panel is not required for the example projects.

For testing the example project some inputs require to be connected as follows:

Fig. 4: Wiring of training case

training_case_TA5450_electrical_connection02

For the example projects, not all input switches and none of the potentiometers included in the training case are necessary.

Switch I1 is required for the example project for central I/O expansion.

Switch I5 is required for the example project for remote I/O expansion.