Converting an AC500 V2 project to an AC500 V3 OPC UA projectPermalink

Application example

A project configured for an AC500 V2 PLC can be converted to an AC500 V3 PLC project. The conversion is mainly performed in Automation Builder, however, several steps must be carried out manually. The complete conversion procedure from a V2 project to a V3 project is described in an ‎⮫ application note.

The application example ‎⮫ AC500 V2 to V3 migration with Modbus describes how to upgrade Modbus TCP or RTU projects from AC500 V2 to AC500 V3.