The editor of the CODESYS Ladder is a network-based editor for the IEC programming language Ladder Diagram (LD).
The main difference as compared with the CODESYS LD FBD editor (which is still available) is the simplified editing capabilities. Variants of elements which previously required separate elements to be inserted from the toolbox are now created purely by the selected insertion position or by subsequently switching a modifier.
Blocks which have been created in the CODESYS LD FBD editor can be converted to the CODESYS Ladder format by means of a menu command.