You can view the PLC log on this tab of the generic device editor. It lists the events that were recorded on the target system. This concerns the following:
- 
                           
Events during the startup and shutdown of the system (components loaded, with version)
 - 
                           
Application download and loading of the boot application
 - 
                           
Custom entries
 - 
                           
Log entries from I/O drivers
 - 
                           
Log entries from data sources
 
The “Log” tab also opens when you click “Open Log Page”. You can configure this as a menu command in the “Customize” dialog.
![]()  | 
                              
                                  Refreshes the list of log events for all runtime system component  | 
                           
| 
                                  “Components”  | 
                              
                                  Filters the display of log events by the runtime system components selected in the list box Example: 
 “<all components>”: Displays the reported events of all components  | 
                           
| 
                                  
  | 
                              
                                  Loads the next page with newer log messages  | 
                           
| 
                                  
  | 
                              
                                  Loads the previous page with older log messages  | 
                           
| 
                                  
  | 
                              
                                  Loads the page with the newest log entries and enables automatic scrolling  | 
                           
| 
                                  
  | 
                              
                                  
 Hint: This is also displayed on the status bar as “Auto-Scroll: ON”.  | 
                           
| 
                                  
  | 
                              
                                  Loads the page with oldest log messages  | 
                           
| 
                                  
  | 
                              
                                  Filters events with the severity “Warning” and notifies about how many Blue-outlined button: Warnings are displayed.  | 
                           
| 
                                  
  | 
                              
                                  Filters events with the severity “Error” and notifies about how many Blue-outlined button: Errors are displayed.  | 
                           
| 
                                  
  | 
                              
                                  Filters events with the severity “Exception” and notifies about how many Blue-outlined button: Exceptions are displayed.  | 
                           
| 
                                  
  | 
                              
                                  Filters events with the severity “Information” and notifies about how many Blue-outlined button: Information is displayed.  | 
                           
| 
                                  
  | 
                              
                                  Filters events with the severity “Debug” and notifies about how many Blue-outlined button: Debug messages are displayed.  | 
                           
| 
                                  Logger  | 
                              
                                  Enables a logger for displaying its recorded events By default, the   | 
                           
| 
                                  “UTC time”  | 
                              
                                  
 
 If you change the option, then the displayed time stamp is converted automatically.  | 
                           
![]()  | 
                              
                                  Exports the list contents to an xml file. You can select the file name and location.  | 
                           
![]()  | 
                              
                                  Imports an XML file with log messages stored in the file system . A separate window opens to display the log messages.  | 
                           
| 
                                  Tabular display of the log messages Ten thousand log messages are displayed per page.  | 
                           |
| 
                                  “Severity”  | 
                              
                                 
  | 
                           
| 
                                  “Time Stamp”  | 
                              
                                  Date and time of the development system or of the runtime system) Example:   | 
                           
| 
                                  “Description”  | 
                              
                                  Description of the event Example:   | 
                           
| 
                                  “Component”  | 
                              
                                  Runtime component where the reported event occurred  | 
                           
| 
                                  “Auto-Scroll”  | 
                              
                                  Displays whether auto-scrolling is enabled (“ON”) or disabled (“OFF”) Hint: Click the  
  | 
                           
Note for error checking
For exceptions with the description *SOURCEPOSITION*, the affected function opens in the editor by double-clicking it or by means of the
                           “Display Source Code in Editor” command in the context menu. The cursor jumps to the line that is causing the error.
                           You can also perform this diagnosis when you have the CODESYS project archive, including the download information files and the exported log file.
                           When the affected function is protected, then the following message appears: "The source code is not available for <function name>".
If a VendorException is reported, then a manufacturer-specific exception error has occurred in the CODESYS runtime. Contact the PLC manufacturer for more information.











: Converts the times displayed below 
: Displays the original time stamp of the runtime system