Symbol: 
Function: This object contains the configuration of the project.
Call:
- 
                           
“Project Project Settings”
 - 
                           
Double-click on the object in the device tree
 
CODESYS saves the project settings directly in the project. If, for example, you transfer a project to another system, the “Project Settings” object is also transferred with it without a project archive being required.
The project settings are valid project-wide and offer setting possibilities for various categories such as “AS” or “Users and Groups”. The available categories vary, depending on which software packages you have installed via the package manager.
See also